AXIS#.CANOPEN.GEARPRIMARY.MOTORREV

Description

This keyword provides the count of motor shaft revolutions for the primary position gearing ratio calculation. It is part of the scaling calculation used for CANOpenClosedCANopen is a communication protocol and device profile specification for embedded systems used in automation for fieldbuses working in real time objects.

Context

See Scaling.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 4294967295

Default Value

1

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

CANBus and EtherCat

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

CANopen

Index

6091h

Subindex

1

Data Type

U32

Float Scale

1:1

Access

Read/Write

PDO Map No